Read/Write |
About the Handler I/O Connector |
Description |
Determines the control of Material Handler connector Pin 20. |
VB Syntax |
handler.IndexState = value |
Variable |
(Type) - Description |
|
handler |
(object) - A Handler I/O object |
|
value |
(boolean) False - Pin 20 is controlled by Output Port B6 True - Pin 20 is controlled by the Index signal |
Return Type |
Boolean |
Default |
False |
Examples |
handler.IndexState = False 'Write bState = handler.IndexState 'Read |
C++ Syntax |
HRESULT put_IndexState (BOOL *pVal); HRESULT get_IndexState (BOOL newVal); |
Interface |
IHWMaterialHandlerIO2 |