Write/Read |
About External DC Devices |
Description |
Sets and returns the Enable I/O command for an external DC Source and an external DC Meter. |
VB Syntax |
extDC.InitCmd = value |
Variable |
(Type) - Description |
|
extDC |
A ExternalDCDevice (object) |
|
value |
(String) The SCPI command used to enable the DC Source and DC Meter. |
Return Type |
String |
Default |
" " Empty String |
Examples |
extDC.InitCmd = "OUTP ON" 'Write value = extDC.InitCmd 'Read |
C++ Syntax |
HRESULT get_InitCmd( BSTR* cmd); HRESULT put_InitCmd( BSTR cmd); |
Interface |
IExternalDCDevice3 |