Write/Read |
About Mixer Configuration |
Description |
Sets or returns the denominator value of the Input Fractional Multiplier. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. |
VB Syntax |
obj.InputDenominator = value |
Variable |
(Type) - Description |
|
obj |
A Mixer Interface pointer to the Measurement (object) Or |
|
value |
(Long) - Input denominator value. |
Return Type |
Long |
Default |
1 |
Examples |
Print mixer.InputDenominator 'prints the value of the InputDenominator |
C++ Syntax |
HRESULT get_InputDenominator(long *pVal) HRESULT put_InputDenominator(long newVal) |
Interface |
IMixer IConverter |