Write/Read |
About Mixer Configuration |
Description |
Specifies whether to use the Input frequency that is greater than the LO or less than the LO. To learn more, see the mixer setup dialog box help. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. |
VB Syntax |
obj.IsInputGreaterThanLO (LO) = bool |
Variable |
(Type) - Description |
|
obj |
A Mixer Interface pointer to the Measurement (object) Or |
|
LO |
(Integer) - LO stage number Choose from 1 (default) or 2 |
|
bool |
(Boolean) - True - Use the Input that is Greater than the specified LO. False - Use the Input that is Less than the specified LO. |
Return Type |
Boolean |
Default |
True |
Examples |
mixer.IsInputGreaterThanLO(1) = True |
C++ Syntax |
HRESULT get_IsInputGreaterThanLO(VARIANT_BOOL * val); HRESULT put_IsInputGreaterThanLO(VARIANT_BOOL val); |
Interface |
IMixer2 IConverter |