Write/Read |
About Gain Compression |
Description |
Set and read the input power at which Linear Gain and all S-parameters are measured. |
VB Syntax |
gca.InputLinearPowerLevel = value |
Variable |
(Type) - Description |
|
gca |
A GainCompression (object) |
|
value |
(double) Linear input power level in dBm. Choose a value from +30 to (-30). |
Return Type |
Double |
Default |
- 25 dBm |
Examples |
gca.InputLinearPowerLevel = -10 'Write |
|
LinPwr = gca.InputLinearPowerLevel 'Read |
|
C++ Syntax |
HRESULT get_InputLinearPowerLevel(double* pVal) HRESULT put_InputLinearPowerLevel(double newVal) |
Interface |
IGainCompression |