Write/Read |
About Receiver Cal |
Description |
Note: This property is replaced by DoReceiverPowerCal Method. Turns ON and OFF normalization interpolation which calculates new divisor data when stimulus values change after normalization. When this property is ON and normalization is being applied, the Normalization algorithm attempts to interpolate the divisor data whenever the stimulus parameters are changed. When this property is OFF under the same circumstances, normalization is turned OFF. Normalization is currently supported only on measurements of unratioed power for the purpose of performing a receiver power calibration. |
VB Syntax |
meas.InterpolateNormalization = value |
Variable |
(Type) - Description |
|
meas |
(object) - A Measurement object |
|
value |
(boolean) False – Turns normalization interpolation OFF True – Turns normalization interpolation ON |
Return Type |
Boolean |
Default |
False -OFF |
Examples |
meas.InterpolateNormalization = False 'Write |
|
normalized = meas.InterpolateNormalization 'Read |
|
C++ Syntax |
HRESULT put_InterpolateNormalization(VARIANT_BOOL bState); HRESULT get_InterpolateNormalization(VARIANT_BOOL *bState); |
Interface |
IMeasurement |