Read-only |
About the ExtTestSetIO connector |
Description |
Reads the boolean that represents the state of the Interrupt In line (pin 13) on the external test set connector. |
VB Syntax |
value = ExtIO.Interrupt |
Variable |
(Type) - Description |
|
value |
(boolean) - Variable to store the returned data |
|
ExtIO |
(object) - An ExternalTestSetIO object |
Return Type |
Boolean False - indicates the line is being held at a TTL High True - indicates the line is being held at a TTL Low |
Default |
Not Applicable |
Examples |
value = ExtIO.Interrupt |
C++ Syntax |
HRESULT get_Interrupt( VARIANT_BOOL* bValue); |
Interface |
IHWExternalTestSetIO |