Read only |
About ECAL |
Description |
This property replaces IsECALModuleFound Property. Returns true or false depending on whether communication was established between the VNA and the specified ECal module. |
VB Syntax |
modFound = cal.IsECALModuleFoundEx (module) |
Variable |
(Type) - Description |
|
modFound |
(boolean) - Variable to store the returned test result. True - The VNA identified the presence of the specified ECal module. False - The VNA did NOT identify the presence of the specified ECal module. |
|
cal |
(object) - A Calibrator object |
|
module |
(long integer) ECal module. Choose from modules 1 through 8 Use GetECALModuleInfoEx to return the model and serial number of each module. |
Return Type |
Boolean |
Default |
Not applicable |
Examples |
Set cal = pna.ActiveChannel.Calibrator moduleFound = cal.IsECALModuleFoundEx(1) |
C++ Syntax |
HRESULT get_IsECALModuleFoundEx( long moduleNumber, VARIANT_BOOL *bModuleFound); |
Interface |
ICalibrator4 |