Read/Write |
About ECAL |
Description |
Value by which to increment (increase) the channel's averaging factor during measurement of isolation in an ECal calibration. Note: If <value> is greater than 1 and the channel currently has averaging turned OFF, averaging will be turned ON only during the isolation measurements and with the averaging factor equal to <value>. |
VB Syntax |
cal.IsolationIncrementAveraging = value |
Variable |
(Type) - Description |
|
cal |
A Calibrator (object) |
|
value |
(Long) Incremental Averaging factor. The maximum averaging factor is 65536 (2^16). |
Return Type |
Long Integer |
Default |
8 |
Examples |
oCal.IsolationAveragingIncrement = 16 'Write |
|
avgIncr = oCal.IsolationAveragingIncrement ' Read |
|
C++ Syntax |
HRESULT get_IsolationAveragingIncrement(long *pVal); HRESULT put_IsolationAveragingIncrement(long newVal); |
Interface |
ICalibrator7 |