Write/Read |
About Mixer Configuration |
Description |
Sets or returns the LO sweep mode. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. Note: There is also a LORangeMode on the Mixer Interface |
VB Syntax |
obj.LORangeMode (n) = value |
Variable |
(Type) - Description |
|
obj |
|
|
n |
(Long) - LO stage number. Choose from 1 or 2 |
|
value |
(Enum as NARangeMode) - LO sweep mode. Choose from: 0 - naSwept 1 - naFixed |
Return Type |
Enum |
Default |
0 - naSwept |
Examples |
mixer.LORangeMode(1)=naSwept |
C++ Syntax |
HRESULT get_LORangeMode(long LO, enum *pVal ) HRESULT put_LORangeMode(long LO, enum newVal) |
Interface |
IConverter |