Write/Read |
About Mixer Configuration |
Description |
Sets or returns the number of LO stages present in the mixer. |
VB Syntax |
obj.LOStage = value |
Variable |
(Type) - Description |
|
obj |
A Mixer Interface pointer to the Measurement (object) Or |
|
value |
(Long) - Number of LO stages. Choose from 1 or 2 |
Return Type |
Long |
Default |
1 |
Examples |
mixer.LOStage = 1 'sets the LO Stage value to 1 |
C++ Syntax |
HRESULT get_LOStage(long *pVal) HRESULT put_LOStage(long newVal) |
Interface |
IMixer IConverter |