Write/Read |
About Mixer Configuration |
Description |
Sets or returns the LO start frequency value. This command can only be used with SMC (not VMC) measurements. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. |
VB Syntax |
obj.LOStartFrequency (n) = value |
Variable |
(Type) - Description |
|
obj |
A Mixer Interface pointer to the Measurement (object) Or |
|
value |
(double) - LO Start Frequency in Hertz. |
|
n |
(Long) - LO stage number Choose from 1 or 2 |
Return Type |
Double |
Default |
Not Applicable |
Examples |
Print mixer.LOStartFrequency(1) 'prints the value of the first LO start frequency |
C++ Syntax |
HRESULT get_LOStartFrequency(long id, double *pVal) HRESULT put_LOStartFrequency(long id,double newVal) |
Interface |
IMixer3 IConverter |