Write/Read |
About Swept IMDx |
Description |
Sets or returns the Start value of a LO Power sweep.. Also set imdx.SweepType to naIMDLOPowerSweep. |
VB Syntax |
obj.LOStartPower (n) = value |
Variable |
(Type) - Description |
|
obj |
|
|
n |
(Long) - LO stage number. Choose 1 |
|
value |
(double) - LO start power in dBm. |
Return Type |
Double |
Default |
-20 dBm |
Examples |
convtr.LOStartPower(1) = -5 'Sets the LO Power sweep start value start = convtr.LOStartPower(1) 'Reads the start value |
C++ Syntax |
HRESULT get_LOStartPower(long LOStage, double *pVal) HRESULT put_LOStartPower(long LOStage, double newVal) |
Interface |
IConverter |