Write/Read |
About Receiver Leveling |
Description |
Sets and returns the IFBW to be used for leveling sweeps. Enable separate IFBW for leveling sweeps using FastMode Property. |
VB Syntax |
RxLevel.LevelingIFBW(srcPort) = value |
Variable |
(Type) - Description |
|
RxLevel |
A ReceiverLeveling Object |
|
srcPort |
(Long Integer) Source port for which to set the LevelingIFBW for Receiver Leveling. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Double) IFBW for leveling sweeps in Hz. The list of valid IF Bandwidths is different depending on the VNA model. See list. If an invalid number is specified, the VNA will round up to the closest valid number. |
Return Type |
(Double) |
Default |
100 kHz |
Examples |
rxLevel.LevelingIFBW (1) = 1e3 ' Write |
|
value = rxLevel.LevelingIFBW 2' Read |
|
C++ Syntax |
HRESULT get_LevelingIFBW(long port, double* pVal); HRESULT put_LevelingIFBW(long port, double newVal); |
Interface |
IReceiverLevelingConfiguration |