Read-only |
About Limits |
Description |
Returns the number of segments used in a limit test. All segments are counted, whether they are on or not. |
VB Syntax |
value = limitst.SegmentCount |
Variable |
(Type) - Description |
|
value |
(Long integer) Variable in which to store the returned segment count. |
|
limitst |
A LimitTest (object) |
Return Type |
Long integer |
Default |
1 Segment is created on new limit test objects. |
Examples |
count=limitst.SegmentCount |
C++ Syntax |
HRESULT get_SegmentCount(long *value); |
Interface |
ILimitTest |