Write/Read |
About Ext Pulse Gens |
Description |
Sets and returns the load impedance of the pulse generator. |
VB Syntax |
extPulseGen.LoadImpedance = value |
Variable |
(Type) - Description |
|
extPulseGen |
An ExternalPulseGenerator (object) |
|
value |
(Double) Pulse generator load impedance. |
Return Type |
Double |
Default |
50 |
Examples |
extPulseGen.LoadImpedance = 50 'Write |
|
load = extPulseGen.LoadImpedance 'Read |
|
C++ Syntax |
HRESULT get_LoadImpedance (double *pValue) HRESULT put_LoadImpedance (double newVal) |
Interface |
IExternalPulseGenerator |