Description |
Prevents use of the mouse, keyboard, and front panel while your program is running. Use of these controls while this property is set TRUE causes an error message on the VNA display. To prevent these messages, see About Error Messages. |
VB Syntax |
app.LocalLockoutState = bool |
Variable |
(Type) - Description |
|
app |
An Application (object) |
|
bool |
(boolean) -Choose either: False - User Interface is NOT locked out. True - User Interface IS locked out. |
Return Type |
Boolean |
Default |
False |
Examples |
app.LocalLockoutState = True 'Write |
|
block = app.LocalLockoutState 'Read |
|
C++ Syntax |
HRESULT get_LocalLockoutState(VARIANT_BOOL *State); |
Interface |
IApplication4 |