Write/Read |
About Limit Lines |
Description |
Set and return whether the Coupled Markers setting controls the ON|OFF state of markers that are coupled. Learn more about Coupled Markers. Refer also to CoupledMarkers Property. |
VB Syntax |
pref.MarkCoupControlsMkrState = value |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
value |
(Boolean) - Choose from: True - With Coupled Markers ON, when a marker is turned on, the same-numbered marker on all coupled traces will also be turned on. Likewise, turning off a marker will turn it off on all coupled traces. False - Turning a marker on or off will have no effect on the markers on other traces. |
Return Type |
Boolean |
Default |
False |
Examples |
pref.MarkCoupControlsMkrState = True 'Write |
|
value = pref.MarkCoupControlsMkrState 'Read |
|
C++ Syntax |
HRESULT get_MarkCoupControlsMkrState (VARIANT_BOOL* preference); HRESULT put_MarkCoupControlsMkrState (VARIANT_BOOL val) |
Interface |
IPreferences15 |