Write/Read |
About Marker Readout |
Description |
Sets the number of marker readouts to display per trace. Display up to 20 marker readouts per window. |
VB Syntax |
win.MarkerReadoutsPerTrace = value |
Variable |
(Type) - Description |
|
win |
A NAWindow (object) |
|
value |
(Long Integer) Number of marker readouts to display. Choose a value between 1 and 10. |
Return Type |
Long Integer |
Default |
5 |
Examples |
win.MarkerReadoutsPerTrace = 3 'Write value = app.ActiveNAWindow.MarkerReadoutsPerTrace 'Read |
C++ Syntax |
HRESULT get_MarkerReadoutsPerTrace(long *pVal) HRESULT put_MarkerReadoutsPerTrace(long newVal) |
Interface |
INAWindow3 |