Write/Read |
About Marker Readout |
Description |
Specifies whether or not to force marker symbols to be displayed above the trace. When ON, all marker symbols will be displayed above the trace and the active marker will be filled solid. |
VB Syntax |
win.MarkerSymbolsAboveTrace = value |
Variable |
(Type) - Description |
|
win |
A NAWindow (object) |
|
value |
(Boolean) False - ONLY the active marker is displayed above the trace. Inactive markers are displayed below the trace. True - ALL marker symbols are displayed above the trace. The active marker is always filled solid. |
Return Type |
Boolean |
Default |
OFF (ON in IM Spectrum and SA measurement classes) |
Examples |
win.MarkerSymbolsAboveTrace = True 'Write value = app.ActiveNAWindow.MarkerSymbolsAboveTrace 'Read |
C++ Syntax |
HRESULT get_MarkerSymbolsAboveTrace(VARIANT_BOOL* pbState) HRESULT put_MarkerSymbolsAboveTrace(VARIANT_BOOL bState) |
Interface |
INAWindow4 |