Write/Read |
About External DC Devices |
Description |
Sets and returns the "Define Max As" ON/OFF state for an external DC Source. |
VB Syntax |
extDC.MaxOutputState = value |
Variable |
(Type) - Description |
|
extDC |
An ExternalDCDevice (object) |
|
value |
(Boolean) "Define Max As" ON/OFF state. Choose from: True - Turn "Define Max As" ON False - Turn "Define Max As" OFF |
Return Type |
Boolean |
Default |
True |
Examples |
extDC.MaxOutputState = True 'Write |
|
value = extDC.MaxOutputState 'Read |
|
C++ Syntax |
HRESULT get_MaxOutputState(VARIANT_BOOL *value) HRESULT put_MaxOutputState(VARIANT_BOOL value) |
Interface |
IExternalDCDevice3 |