Read/Write |
About Embedded LO |
Description |
Sets and returns the maximum number of tuning iterations to achieve the precise tolerance. |
VB Syntax |
obj.MaxPreciseTuningIterations = value |
Variable |
(Type) - Description |
|
obj |
An EmbeddedLO (object) or A ConverterEmbeddedLO (object) |
|
value |
(Long) Maximum number of tuning iterations. |
Return Type |
(Long) |
Default |
5 |
Examples |
embedLO.MaxPreciseTuningIterations = 3 'write |
|
value = embedLO.MaxPreciseTuningIterations 'read |
|
C++ Syntax |
HRESULT get_MaxPreciseTuningIterations long* iter); HRESULT put_MaxPreciseTuningIterations long iter); |
Interface |
IEmbededLO |