Read/Write |
About Dynamic Uncertainty |
Description |
Sets and returns the maximum number of points for which uncertainties are to be computed for subsequent calibrations that are performed using Dynamic Uncertainty. |
VB Syntax |
uncertMan.MaximumUncertaintyPoints = value |
Variable |
(Type) - Description |
|
uncertMan |
An UncertaintyManager Object |
|
value |
(Boolean) Max number of points. |
Return Type |
Long Integer |
Default |
500 |
Examples |
uncertMan.MaximumUncertaintyPoints = 201 |
C++ Syntax |
HRESULT get_MaximumUncertaintyPoints([out,retval] long* pNumPoints); HRESULT put_MaximumUncertaintyPoints([in] long numPoints); |
Interface |
IUncertaintyManager |