Read-only |
About Trace Statistics |
Description |
Returns the mean value of the measurement . To retrieve all 3 statistics value at the same time, use meas.GetTraceStatistics |
VB Syntax |
average = meas.Mean |
Variable |
(Type) - Description |
|
average |
(single) - Variable to store mean value |
|
meas |
A Measurement (object) |
Return Type |
Single |
Default |
Not applicable |
Examples |
Dim average as Single |
C++ Syntax |
HRESULT get_Mean(float* mean) |
Interface |
IMeasurement |