Read only |
About Measurement Classes |
Description |
Provides access to the MeasurementClassProperties Object. |
VB Syntax |
handle = cap.MeasurementClassProperties (measClass) |
Variable |
(Type) - Description |
|
handle |
(Variant) - Variable to store the returned object. |
|
cap |
A Capabilities (object) |
|
measClass |
(String) Name of the measurement class to be accessed. Use AvailableMeasurementClasses Property to return a list of measurement classes installed on the VNA. |
Return Type |
Object |
Default |
Not Applicable |
Examples |
'Access the MeasurmentClassProperties Object Set app = CreateObject("AgilentPNA835x.Application") Set cap = app.Capabilities Set measProps = cap.MeasurmentClassProperties("SweptIMD") |
C++ Syntax |
HRESULT put_MeasurementClassProperties(IMeasurementClassProperties *handle); |
Interface |
ICapabilities8 |