Write/Read |
About Traces |
Description |
Sets (or returns) the Name of the measurement. Measurement names must be unique among the set of measurements. Measurement names cannot be an empty string. Note: This is the same name as trace.Name; when one changes, the other changes. |
VB Syntax |
meas.Name = value |
Variable |
(Type) - Description |
|
meas |
A Measurement (object) |
|
value |
(string) - A user defined name of the measurement |
Return Type |
String |
Default |
"CH1_S11_1" - name of the default measurement |
Examples |
meas.Name = "Filter BPass" 'Write |
|
MName = meas.Name 'Read |
|
C++ Syntax |
HRESULT get_Name(BSTR *pVal) |
Interface |
IMeasurement |