Read-Write |
About FCA embed/deembed |
Description |
Specifies the S2P filename to embed or de-embed on the input or output of your mixer measurement. |
VB Syntax |
object.NetworkFilename(n) = filename |
Variable |
(Type) - Description |
|
object |
SMCType (object) or VMCType (object) |
|
n |
(Integer) Apply network to input or output of mixer. Choose from: 1 - Input of mixer 2 - Output of mixer |
|
filename |
(String) Filename of the S2P used for embedding or de-embedding. Use the full path name, file name, and .S2P suffix, enclosed in quotes. |
Return Type |
String |
Default |
Not Applicable |
Examples |
VMC.Filename(2) = "D:\WaveguideAdapt.S2P" |
C++ Syntax |
HRESULT put_NetworkFilename(short networkNum, BSTR filename); HRESULT get_NetworkFilename(short networkNum, BSTR *filename); |
Interface |
SMCType2 VMCType2 |