Read-Write |
About FCA embed/deembed |
Description |
Allows you to embed (add) or de-embed (remove) circuit network effects on the input and output of your mixer measurement. |
VB Syntax |
object.NetworkMode(n) = value |
Variable |
(Type) - Description |
|
object |
SMCType (object) or VMCType (object) |
|
n |
(Integer) Apply network to input or output of mixer. Choose from: 1 - Input of mixer 2 - Output of mixer |
|
value |
(ENum as ENetworkMode) Choose from: NO_NETWORK Do nothing with effects of S2P file EMBED_NETWORK - Add effects of S2P file from the measurement results. DEEMBED_NETWORK - Remove effects of S2P file from the measurement results. |
Return Type |
Enum |
Default |
NO_NETWORK |
Examples |
VMC.NetworkMode = EMBED_NETWORK |
C++ Syntax |
HRESULT put_NetworkMode(short networkNum, enum ENetworkMode networkMode); HRESULT get_NetworkMode(short networkNum, enum ENetworkMode *networkMode); |
Interface |
SMCType2 VMCType2 |