Write/Read |
About Noise Figure |
Description |
Sets and returns the temperature of the noise source connector. |
VB Syntax |
noise.NoiseSourceCold = value |
Variable |
(Type) - Description |
|
noise |
A NoiseCal (object) |
|
value |
(double) Noise source temperature in Kelvin. |
Return Type |
Double |
Default |
Not Applicable |
Examples |
noise.NoiseSourceCold = 295 'Write |
|
temp = noise.NoiseSourceCold 'Read |
|
C++ Syntax |
HRESULT get_NoiseSourceCold(double* pTemp) HRESULT put_NoiseSourceCold(double pNewTemp) |
Interface |
INoiseCal |