Write/Read |
About Mixer Configuration |
Description |
Toggles the Nominal Incident Power setting ON and OFF. This setting is ONLY to be used with SMC measurements, not VMC. Learn more about Nominal Incident Power. |
VB Syntax |
mixer.NominalIncidentPowerState = bool |
Variable |
(Type) - Description |
|
mixer |
A Mixer (object) |
|
bool |
(boolean) - Nominal Incident Power State. Choose from: 1 -(True) Turn nominal incident power ON 0 -(False) Turn nominal incident power OFF |
Return Type |
Boolean |
Default |
0 -(False) |
Examples |
mixer.NominalIncidentPowerState = True 'sets NominalIncidentPowerState to ON |
C++ Syntax |
HRESULT get_NominalIncidentPowerState(VARIANT_BOOL *pVal) HRESULT put_NominalIncidentPowerState(VARIANT_BOOL val ); |
Interface |
IMixer4 |