Write/Read |
About Receiver Cal |
Description |
Note: This property is replaced by DoReceiverPowerCal Method. Sets or returns normalization ON or OFF for the measurement. Normalization is currently supported only on measurements of unratioed power for the purpose of performing a receiver power calibration. If this property is set to ON for a ratioed measurement (such as S-parameter), it will return an error. This property will also return an error when set to ON if the divisor buffer doesn’t yet exist. |
VB Syntax |
meas.Normalization = value |
Variable |
(Type) - Description |
|
meas |
(object) - A Measurement object |
|
value |
(boolean) False – Turns normalization OFF True – Turns normalization ON |
Return Type |
Boolean |
Default |
False |
Examples |
meas.Normalization = False 'Write |
|
normalized = meas.Normalization 'Read |
|
C++ Syntax |
HRESULT put_Normalization(VARIANT_BOOL bState); HRESULT get_Normalization(VARIANT_BOOL *bState); |
Interface |
IMeasurement |