Read/Write |
About Embedded LO |
Description |
Sets and returns the sweep data point around which to perform broadband and precise tuning. |
VB Syntax |
obj.NormalizePoint = value |
Variable |
(Type) - Description |
|
obj |
An EmbeddedLO (object) or A ConverterEmbeddedLO (object) |
|
value |
(Long) Mixer Sweep data point. Choose a data point number between 1 and the max number of data points in the sweep that has the least amount of expected noise. |
Return Type |
(Long) |
Default |
Center point in the sweep span |
Examples |
embedLO.NormalizePoint = 101 'write |
|
value = embedLO.NormalizePoint 'read |
|
C++ Syntax |
HRESULT get_NormalizePoint(long *point); HRESULT put_NormalizePoint(long point); |
Interface |
IEmbededLO |