Read-only |
About Embedded LO |
Description |
Returns the number of tuning sweeps used for the latest embedded LO measurement. |
VB Syntax |
value = embedLODiag.NumberOfSweeps |
Variable |
(Type) - Description |
|
value |
(Long) Variable to store the returned data. |
|
embedLODiag |
An EmbeddedLODiagnostic (object) |
Return Type |
(Long) |
Default |
Not Applicable |
Examples |
data= embedLODiag.NumberOfSweeps 'read |
C++ Syntax |
HRESULT get_NumberOfSweeps(long * numSweeps); |
Interface |
IEmbededLODiagnostic |