Read-only |
About Auxiliary Triggering |
Description |
Returns the number of the Auxiliary Trigger connector pair currently being used with the instance of the AuxTrigger object. Set the trigger pair with the AuxTrig object. |
VB Syntax |
value = auxTrig.Number |
Variable |
(Type) - Description |
|
auxTrig |
An AuxTrigger (object) |
|
value |
(Long Integer) - Connector pair. PNA-X returns 1 or 2. All other models that do not have the Aux trigger connector returns 1. |
Return Type |
Single |
Default |
Not Applicable |
Examples |
value = auxTrig.Number 'Read the value |
C++ Syntax |
HRESULT get_Number(long *auxID); |
Interface |
IAuxTrigger |