Read-only |
About Measurements |
Description |
Returns the Number of the measurement. Measurement numbers are assigned internally. Note: Measurement numbers are NOT the same as their number in the Measurements collection. Measurement number is used to identify the measurement associated with an event. This property is used to identify measurements when events occur through the OnMeasurementEvent callback. For example: OnMeasurementEvent (naEventId_MSG_LIMIT_FAILED, 3) |
VB Syntax |
measNum = meas.Number |
Variable |
(Type) - Description |
|
measNum |
(long) - variable to store the measurement number |
|
meas |
A Measurement (object) |
Return Type |
Long Integer |
Default |
"1" - number of the default measurement |
Examples |
measNum = meas.Number |
C++ Syntax |
HRESULT get_Number(long *MeasurementNumber) |
Interface |
IMeasurement |