Read-only |
|
Description |
Returns the number of data points of the measurement. To understand how this property is useful, see IMeasurement2 Interface. |
VB Syntax |
value = meas.NumberOfPoints |
Variable |
(Type) - Description |
|
value |
(Long) - variable to store the returned value |
|
meas |
A Measurement (object) |
Return Type |
Long Integer |
Default |
Not Applicable |
Examples |
Print meas.NumberOfPoints 'prints the number of data points |
C++ Syntax |
HRESULT get_NumberOfPoints(long *pVal); |
Interface |
IMeasurement2 |