Write/Read |
About Spectrum Analyzer Markers |
Description |
Sets and returns the occupied bandwidth on/off state. |
VB Syntax |
mkr.OccupiedBandState = value |
Variable |
(Type) - Description |
|
mkr |
A Marker (object) |
|
value |
(Enum as NaStates) - Choose from: naOFF (0) - Turns occupied bandwidth OFF. naON (1) - Turns occupied bandwidth ON. |
Return Type |
Enum |
Default |
naOFF (0) |
Examples |
mkr.OccupiedBandState = naON 'Write |
|
obwstate = mkr.OccupiedBandState 'Read |
|
C++ Syntax |
HRESULT OccupiedBandState(tag NAStates* pState); |
Interface |
IMarker7 Note: If occupied band state is turned ON, then Band Power or Band Noise is turned OFF. |