Write/Read |
About Receiver Attenuation |
Description |
Set and return whether to offset the reference receiver by the amount of receiver attenuation. Learn more. This setting remains until changed or until the hard drive is changed or reformatted. |
VB Syntax |
pref.OffsetReceiverAttenuator = value |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
value |
(Boolean) - Choose from: False Do NOT offset the test port receivers. True Offset the test port receivers. |
Return Type |
Boolean |
Default |
True PNA-X models False E836xB and PNA-L models |
Examples |
pref.OffsetReceiverAttenuator = 1 'Write |
|
Rcvroffset = pref.OffsetReceiverAttenuator 'Read |
|
C++ Syntax |
HRESULT get_OffsetReceiverAttenuator(VARIANT_BOOL * val); HRESULT put_OffsetReceiverAttenuator(VARIANT_BOOL val); |
Interface |
IPreferences6 |