Write/Read |
About Source Attenuation |
Description |
Set and return whether to mathematically offset the reference receivers by the amount of source attenuation. Learn more. This setting remains until changed or until the hard drive is changed or reformatted. |
VB Syntax |
pref.OffsetSourceAttenuator = value |
Variable |
(Type) - Description |
|
pref |
A Preferences (object) |
|
value |
(Boolean) - Choose from: False Do NOT offset the reference receivers. True Offset the reference receivers. |
Return Type |
Boolean |
Default |
True PNA-X models False E836xB and PNA-L models |
Examples |
pref.OffsetSourceAttenuator = 1 'Write |
|
Rcvroffset = pref.OffsetSourceAttenuator 'Read |
|
C++ Syntax |
HRESULT get_OffsetSourceAttenuator(VARIANT_BOOL * val); HRESULT put_OffsetSourceAttenuator(VARIANT_BOOL val); |
Interface |
IPreferences6 |