Write/Read |
About Ext Pulse Gens |
Description |
Sets and returns the output channel of the pulse generator. |
VB Syntax |
extPulseGen.OutputChannel = value |
Variable |
(Type) - Description |
|
extPulseGen |
An ExternalPulseGenerator (object) |
|
value |
(Long) Pulse Generator output port. Choose from 1 or 2. |
Return Type |
Long Integer |
Default |
1 |
Examples |
extPulseGen.OutputChannel = 2 'Write |
|
port = extPulseGen.OutputChannel 'Read |
|
C++ Syntax |
HRESULT get_OutputChannel (long *pValue) HRESULT put_OutputChannel (long newVal) |
Interface |
IExternalPulseGenerator |