Write/Read |
About Mixer Configuration |
Description |
Sets or returns the mixer Output Stop frequency. If you are changing several mixer configuration settings, you can make all the changes first and then issue the Calculate and Apply commands as you would do from the user interface. |
VB Syntax |
obj.OutputStopFrequency = value |
Variable |
(Type) - Description |
|
obj |
A Mixer Interface pointer to the Measurement (object) Or |
|
value |
(double) - Output stop frequency in Hertz. |
Return Type |
Double |
Default |
Not Applicable |
Examples |
Print mixer.OutputStopFrequency 'prints the value of the OutputStopFrequency |
C++ Syntax |
HRESULT get_OutputStopFrequency(double *pVal) HRESULT put_OutputStopFrequency(double newVal) |
Interface |
IMixer IConverter |