Read-only |
About PNOP / PSAT Marker Search |
Description |
Returns the PMaxOut result of the PNOP and PSAT marker search. PMaxOut = Marker 3 Y-axis value |
VB Syntax |
pMaxOut = pMark.PMaxOut |
Variable |
(Type) - Description |
|
pMaxOut |
(double) - Variable to store returned value |
|
pMark |
A PNOP (object) or PSaturation (object) |
Return Type |
Double |
Default |
Not applicable |
Examples |
pMaxOut = pMark.PMaxOut 'Read |
C++ Syntax |
HRESULT get_PMaxOut(double* pNewVal) |
Interface |
IPNOP or IPSaturation |