Description |
Sets and reads the mode of the PassFail line on the HANDLER IO connector (pin 33). Learn more about Global Pass/Fail. |
VB Syntax |
object.PassFailMode = value |
Variable |
(Type) - Description |
|
object |
(object) - An Aux I/O or Handler I/O object |
|
value |
(enum as NAPassFailMode).Choose from: 1 - naDefaultPassWaitMode - the line stays in PASS state. When a device fails, then the line goes to fail after the Sweep End line is asserted. 2 - naDefaultFailWaitMode- the line stays in FAIL state. When a device passes, then the line goes to PASS state after the Sweep End line is asserted. |
Return Type |
Long Integer |
Default |
0 - naDefaultPassNoWaitMode |
Examples |
HWAuxIO.PassFailMode = naDefaultPassNoWaitMode 'Write mode = HWAuxIO.PassFailMode 'Read |
C++ Syntax |
HRESULT put_PassFailMode ( tagNAPassFailMode Mode ); HRESULT get_PassFailMode ( tagNAPassFailMode* Mode ); |
Interface |
IHWAuxIO IHWMaterialHandlerIO |