Write/Read |
About Cal All |
Description |
Allows you to set and return the Path Configuration settings for a Cal All calibration. |
VB Syntax |
calAll.PathConfigurationElement (element).value = setting |
Variable |
(Type) - Description |
|
calAll |
A CalibrateAllChannels (object) |
|
element |
(String) Path configuration element to be set. See a list of configurable RF Path elements. Is this also for IF Path configuration elements? |
|
setting |
(String) Path configuration element setting. |
Return Type |
String |
Default |
Default settings vary with each element. |
Examples |
CalAll.PathConfigurationElement(“Port1NoiseTuner”).value = “Internal” 'returns the PathConfigurationElement setting |
C++ Syntax |
HRESULT put_PathConfigurationElement(BSTR name, IPathElement** pElement); |
Interface |
ICalibrateAllChannels |