Write / Read |
About Path Elements |
Description |
Returns the name of the setting for the given path element name or sets the value of a path element. |
VB Syntax |
powerRange.PathElement (element).value = setting |
Variable |
(Type) - Description |
|
powerRange |
A PowerRange (object) |
|
element |
(String) Path configuration element to be set. See a list of configurable RF Path elements. |
|
setting |
(String) Path configuration element setting. |
Return Type |
String |
Default |
Default settings vary with each element. |
Examples |
powerRange.PathElement("Src2Out1LowBand").value = "HiPwr" |
C++ Syntax |
HRESULT put_PathElement(BSTR name, IPathElement** pElement); |
Interface |
IPowreRange |