Read-only |
About Trace Statistics |
Description |
Returns the Peak to Peak value of the measurement.To retreive all 3 statistics value at the same time, use meas.GetTraceStatistics |
VB Syntax |
pp = meas.PeakToPeak |
Variable |
(Type) - Description |
|
pp |
(single) - Variable to store peak-to-peak value |
|
meas |
A Measurement (object) |
Return Type |
Single |
Default |
Not applicable |
Examples |
pp = meas.PeakToPeak 'Read |
C++ Syntax |
HRESULT get_PeakToPeak(float* pp) |
Interface |
IMeasurement |