Write/Read |
About Marker Search |
Description |
Sets and reads the peak excursion value for the specified marker. The Excursion value determines what is considered a "peak". |
VB Syntax |
mark.PeakExcursion = value |
Variable |
(Type) - Description |
|
mark |
A Marker (object) |
|
value |
(single) - Peak Excursion. Choose any number between -500 and 500 |
Return Type |
Single |
Default |
3 |
Examples |
mark.PeakExcursion = 1 'Write |
|
PkExcur = mark.PeakExcursion 'Read |
|
C++ Syntax |
HRESULT get_PeakExcursion(float *pVal) |
Interface |
IMarker |