Write/Read

Period Property


Description

Sets the pulse-period (1/PRF) for ALL PNA-X internal pulse generators.

The resolution of the period is 16.667nS.

 VB Syntax

pulse.Period = value

Variable

(Type) - Description

pulse

A PulseGenerator (object)

value

(Double)  Pulse period in seconds. Choose a value from about 33ns to about 70 seconds.

Return Type

Double

Default

1e-3 sec

Examples

pulse.Period = 1ms 'Write

value = pulse.Period 'Read

C++ Syntax

HRESULT get_Period(double* period);

HRESULT put_Period(double period);

Interface

IPulseGenerator