Write/Read |
About Phase Control |
Description |
Write and read the Phase Control mode for the specified port. |
VB Syntax |
phase.PhaseControlMode(srcPort) = value |
Variable |
(Type) - Description |
|
phase |
A PhaseControl Object |
|
srcPort |
(Long Integer) Source port for which to make phase control settings. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Enum as NAPhaseControlMode) Choose from: 0 - naPhaseControlOff Do NOT control the phase of <port>. 1 - naPhaseControlParameter Control the phase of <port>. 2 - naPhaseControlReference (READ-only) - reference port for a 'controlled' (parameter) Port. 3 - naPhaseControlOpenLoop Sets a raw phase value for either swept phase or fixed phase, but no receivers are used to control the phase. |
Return Type |
Enum |
Default |
0 - naPhaseControlOff |
Examples |
phase.PhaseControlMode 1 = naPhaseControlParameter ' Write |
|
value = phase.PhaseControlMode 2' Read |
|
C++ Syntax |
HRESULT get_PhaseControlMode(long port, enum NAPhaseControlMode* pVal); HRESULT put_PhaseControlMode(long port, enum NAPhaseControlMode newVal); |
Interface |
IPhaseControl |