Write/Read |
About Phase Control |
Description |
Write and read an array of phase offsets. Each phase offset is summed with each phase point to get new target value. The VNA attempts to set phase for each target value. The number of phase offset values must be the same as the number of data points. |
VB Syntax |
phase.PhaseCorrectionData(srcPort) = value |
Variable |
(Type) - Description |
|
phase |
A PhaseControl Object |
|
srcPort |
(Long Integer) Source port for which to make phase control settings. Note: If the source port is defined by a string name, such as an external source, a balanced port, or one of the Source 2 outputs on the 2-port 2-source PNA-X model, then use chan.getPortNumber to translate the string into a port number. To learn more see Remotely Specifying a Source Port |
value |
(Long values) Phase offset data array. |
Return Type |
Long data array |
Default |
Not Applicable |
Examples |
phase.PhaseCorrectionData 1 = 10,11,12 ' Write 3 phase offset values |
|
value = phase.PhaseCorrectionData 2' Read |
|
C++ Syntax |
HRESULT get_PhaseCorrectionData(long port, long* pVals); HRESULT put_PhaseCorrectionData(long port, long newVals); |
Interface |
IPhaseControl |